Package Information

Package Information 144 CSBGA
Package Code X14422+2C
Outline Number 21-0163
Land Pattern Number 90-0185
Thermal Resistance, Four-Layer Board:
Junction to Ambient (θJA) 25.4°C/W
Junction to Case (θJC) 5.6°C/W

For the latest package outline information and land patterns (footprints), go to www.maximintegrated.com/packages. Note that a “+”, “#”, or “-” in the package code indicates RoHS status only. Package drawings may show a different suffix character, but the drawing pertains to the package regardless of RoHS status.

Package thermal resistances were obtained using the method described in JEDEC specification JESD51-7, using a four-layer board. For detailed information on package thermal considerations, refer to www.maximintegrated.com/thermal-tutorial.

data-opMAX78002GXE%2B
Battery Power Supply. Bypass device pin A10 with a 1μF capacitor placed as close as possible to this pin and the VSSPWR pin. This pin must be connected to VREGI and VDDIOH at the circuit board level.Battery Power Supply for the SIMO Switch-Mode Power Supply (SMPS). Bypass this pin with 2 x 47μF capacitors placed as close as possible to this pin and the VSSPWR pin. This pin must be connected to VBAT and VDDIOH. If the power to the device is cycled, the voltage applied to this pin must reach VREGI_POR.1.8V Analog Power Supply. Bypass this pin with a 1μF capacitor placed as close as possible to this pin and VSSA. This device pin must be connected to VDDIO.USB Transceiver Supply Voltage. Bypass this pin to VSSB with a 1.0μF capacitor as close as possible to the package.ADC External Reference Input. Bypass this pin with a 1μF capacitor placed as close as possible to this pin and VSSA as possible. This is the reference input for the analog-to-digital converter (ADC). If the external reference is not used, tie this pin to VSSA through a 500Ω resistor.Digital Core Supply Voltage A. Bypass this pin to VSS with a 1μF capacitor placed as close to this pin as possible.Digital Core Supply Voltage B. Bypass this pin to VSS with a 1μF capacitor placed as close to this pin as possible.Boosted Supply Voltage for the Gate Drive of High-Side Switches. Bypass VBST to LXB with a 3.3nF capacitor.Buck Converter A Voltage Output. Bypass this pin with a 22μF capacitor to VSS placed as close as possible to this pin.Buck Converter B Voltage Output. Bypass this pin with a 22μF capacitor to VSS placed as close as possible to this pin.Buck Converter C Voltage Output. Bypass this pin with a 22μF capacitor to VSS placed as close as possible to this pin.GPIO Supply Voltage. Bypass this pin to VSS with a 1.0μF capacitor placed as close as possible to the package.GPIO Supply Voltage, High. VDDIOH ≥ VDDIO. Bypass this pin to VSS with a 1.0μF capacitor placed as close as possible to the package. This device pin must be connected to VREGI and VBAT.Bypass with 1μF capacitor to VSSB. Do not connect this device pin to any other external circuitry.Bypass with 1μF capacitor to VSS. Do not connect this device pin to any other external circuitry.Digital Ground.Analog Ground. This pin is the return path for VREF and VDDA.Ground for the SIMO Switch-Mode Power Supply (SMPS). This device pin is the return path for the VREG.USB Transceiver Ground.Switching Inductor Input A. Connect a 2.2μH inductor between LXA and LXB.Switching Inductor Input B. Connect a 2.2μH inductor between LXA and LXB.Voltage Supply for CNN x16 Processor Quadrant 0. Bypass this pin with 3 x 1μF capacitors as close to this pin as possible and a 22μF capacitor as close as possible to the package.Voltage Supply for CNN x16 Processor Quadrant 1. Bypass this pin with 3 x 1μF capacitors as close to this pin as possible and a 22μF capacitor as close as possible to the package.Voltage Supply for CNN x16 Processor Quadrant 2. Bypass this pin with 3 x 1μF capacitors as close to this pin as possible and a 22μF capacitor as close as possible to the package.Voltage Supply for CNN x16 Processor Quadrant 3. Bypass this pin with 3 x 1μF capacitors as close to this pin as possible and a 22μF capacitor as close as possible to the package.Voltage Supply for the RAM for the CNN x16 Processor Quadrant 0. Bypass this pin with 2 x 1μF capacitors as close to this pin as possible and a 22μF capacitor as close as possible to the package.Voltage Supply for the RAM for the CNN x16 Processor Quadrant 1. Bypass this pin with 2 x 1μF capacitors as close to this pin as possible and a 22μF capacitor as close as possible to the package.Voltage Supply for the RAM for the CNN x16 Processor Quadrant 2. Bypass this pin with 2 x 1μF capacitors as close to this pin as possible and a 22μF capacitor as close as possible to the package.Voltage Supply for the RAM for the CNN x16 Processor Quadrant 3. Bypass this pin with 2 x 1μF capacitors as close to this pin as possible and a 22μF capacitor as close as possible to the package.Enable Output for the Voltage Supply for CNN x16 Processor Quadrant 0.Enable Output for the Voltage Supply for CNN x16 Processor Quadrant 1.Enable Output for the Voltage Supply for CNN x16 Processor Quadrant 2.Enable Output for the Voltage Supply for CNN x16 Processor Quadrant 3.Enable Output for the Voltage Supply for the RAM for the CNN x16 Processor Quadrant 0.Enable Output for the Voltage Supply for the RAM for the CNN x16 Processor Quadrant 1.Enable Output for the Voltage Supply for the RAM for the CNN x16 Processor Quadrant 2.Enable Output for the Voltage Supply for the RAM for the CNN x16 Processor Quadrant 3.Active-Low, External System Reset Input. The device remains in reset while this pin is in its active state. When the pin transitions to its inactive state, the device performs a POR reset (resetting all logic on all supplies except for RTC circuitry) and begins execution. This pin has an internal pull-up to the VDDIOH supply.32kHz Crystal Oscillator Output.32kHz Crystal Oscillator Input. Connect a 32kHz crystal between 32KIN and 32KOUT for RTC operation. Optionally, this pin can be configured as the input for an external CMOS-level clock source.25MHz Crystal Oscillator Input. Connect a 25MHz crystal between HFXIN and HFXOUT. Optionally, this pin can be configured as the input for an external CMOS-level clock source.25MHz Crystal Oscillator Output.UART0 Receive Port Map A. See Bootloader Activation for details on this pin's usage and suggested pull-up.UART0 Transmit Port Map A.Timer0 I/O 32 Bits or Lower 16 Bits Port Map A; UART0 Clear to Send Port Map B.External Clock for Use as SYS_OSC/Timer0 I/O Upper 16 Bits Port Map A; UART0 Request to Send Port Map B.SPI0 Port Map A Target Select 0; Timer0 Inverted Output Port Map B.SPI0 Port Map A Controller-Out Target-In Serial Data 0; Timer0 Inverted Output Upper 16 Bits Port Map B.SPI0 Port Map A Controller-In Target-Out Serial Data 1; 1-Wire Controller Data I/O.SPI0 Port Map A Clock; 1-Wire Controller Pull-up Enable Output.SPI0 Port Map A Data 2 I/O; Timer0 I/O 32 Bits or Lower 16 Bits Port Map B.SPI0 Port Map A Data 3 I/O; Timer0 I/O Upper 16 Bits Port Map B.I2C0 Port Map A Clock; SPI0 Target Select 2.I2C0 Port Map A Serial Data; SPI0 Target Select 1.UART1 Receive Port Map A; Timer1 Inverted Output Port Map B.UART1 Transmit Port Map A; Timer1 Inverted Output Upper 16 Bits Port Map B.Timer1 I/O 32 Bits or Lower 16 Bits Port Map A; I2S External Clock Input.Timer1 I/O Upper 16 Bits Port Map A; Parallel Camera Interface Vertical Sync.I2C1 Port Map A Clock; Pulse Train 2.I2C1 Port Map A Serial Data; Pulse Train 3.Pulse Train 0; 1-Wire Controller Data I/O.Pulse Train 1; 1-Wire Controller Pull-up Enable Output.SPI1 Port Map A Target Select 0; Parallel Camera Interface Data 0.SPI1 Port Map A Controller-Out Target-In Serial Data 0; Parallel Camera Interface Data 1.SPI1 Port Map A Controller-In Target-Out Serial Data 1; Parallel Camera Interface Data 2.SPI1 Port Map A Clock; Parallel Camera Interface Data 3.SPI1 Port Map A Data 2; Parallel Camera Interface Data 4.SPI1 Port Map A Data 3; Parallel Camera Interface Data 5.Timer2 I/O 32 Bits or Lower 16 Bits Port Map A; Parallel Camera Interface Data 6.USB External Clock/Timer2 I/O Upper 16 Bits Port Map A; Parallel Camera Interface Data 7.Serial Wire Debug Data I/O. Following any reset, this device pin defaults to AF1 SWDIO.Serial Wire Debug Clock. Following any reset, this device pin defaults to AF1 SWDCLK. See Bootloader Activation for details on this pin's usage and suggested pullup.I2C2 Port Map A Clock; Parallel Camera Interface Data 8.I2C2 Port Map A Serial Data; Parallel Camera Interface Data 9.UART2 Receive Port Map A; 32-bit RISC-V Test Port Clock.UART2 Transmit Port Map A; 32-bit RISC-V Test Port Select.I2S0 Port Map A Bit Clock; 32-bit RISC-V Test Port Data Input.I2S0 Port Map A Left/Right Clock; 32-bit RISC-V Test Port Data Output.I2S0 Port Map A Serial Data Input; Timer3 I/O 32 Bits or Lower 16 Bits Port Map B.I2S0 Port Map A Serial Data Output; Timer3 I/O Upper 16 Bits Port Map B.Timer3 I/O 32 Bits or Lower 16 Bits Port Map A; Parallel Camera Interface Data 10.Timer3 I/O Upper 16 Bits Port Map A; Parallel Camera Interface Data 11.Parallel Camera Interface Horizontal Sync; CM4 Rx Event Input.Parallel Camera Interface Pixel Clock; CM4 Tx Event Output.Secure Digital Interface Card Present; ADC External Clock Input.Secure Digital Interface Data Bus Bit 3.Secure Digital Interface Data Bus Bit 2; ADC Trigger Input A.Secure Digital Interface Data Bus Bit 1; ADC Trigger Input B.Secure Digital Interface Data Bus Bit 0; ADC Trigger Input C.Secure Digital Interface Write Protect.Secure Digital Interface Bus Command.Secure Digital Interface Clock.ADC Input 0/Comparator 0 Negative Input.ADC Input 1/Comparator 0 Positive Input.ADC Input 2/Comparator 1 Negative Input.ADC Input 3/Comparator 1 Positive Input.ADC Input 4/Comparator 2 Negative Input; Low-Power Timer0 I/O Port Map B.ADC Input 5/Comparator 2 Positive Input; Low-Power Timer1 I/O Port Map B.Low-Power Timer0 External Clock Input/ADC Input 6/Comparator 3 Negative Input; Low-Power UART0 Receive Port Map B.Low-Power Timer1 External Clock Input/ADC Input 7/Comparator 3 Positive Input; Low-Power UART Transmit Port Map B.Power-Down Output; Wakeup Input. This device pin can only be powered by VDDIOH.RTC Square-Wave Output; Wakeup Input. This device pin can only be powered by VDDIOH.USB DP Signal. This bidirectional pin carries the positive differential data or single-ended data. This pin is weakly pulled high internally when the USB is disabled.USB DM Signal. This bidirectional pin carries the negative differential data or single-ended data. This pin is weakly pulled high internally when the USB is disabled.MIPI CSI-2 receiver differential clock positive input.MIPI CSI-2 receiver differential clock negative input.MIPI CSI-2 receiver differential data lane 0 positive input.MIPI CSI-2 receiver differential data lane 0 negative input.MIPI CSI-2 receiver differential data lane 1 positive input.MIPI CSI-2 receiver differential data lane 1 negative input.