Depending on the input voltage (VIN = VDD - VSS), the devices operate in four different modes: PD detection, PD classification, mark event, and PD power. The devices enter PD detection mode when the input voltage is between 1.4V and 10.1V. The device enters PD classification mode when the input voltage is between 12.5V and 20.5V. The devices enter PD power mode once the input voltage exceeds VON.
Detection Mode
In detection mode, the power source equipment (PSE) applies two voltages on VIN in the 1.4V to 10.1V range (1V step minimum) and then records the current measurements at the two points. The PSE then computes ΔV/ΔI to ensure the presence of the 24.9kΩ signature resistor.
In detection mode, most of device internal circuitry is off and the offset current is less than 10μA. If the voltage applied to the PD is reversed, install protection diodes at the input terminal to prevent internal damage to the devices (see the Typical Application Circuit). Since the PSE uses a slope technique (ΔV/ΔI) to calculate the signature resistance, the DC offset due to the protection diodes is subtracted and does not affect the detection process.
Classification Mode
In the classification mode, the PSE classifies the PD based on the power consumption required by the PD. This allows the PSE to efficiently manage power distribution. Two external resistors connected CLSA/CLSB to VSS set classification signature to the PSE and define the power consumption requested from the PD. RCLSA sets classification current for the 1st and 2nd class events for 0~4 class PD complaint with IEEE 802.3af/at standard, and RCLSB set classification current for the 3rd to 5th class event for 0~8 class PD complaint with IEEE 802.3bt standard.
The PSE classifies the PD by applying a voltage at the PD input and measuring the current sourced out of the PSE. When the PSE applies a voltage between 12.5V and 20.5V, the devices exhibit a series of events with current characteristic. Table 1 shows the RCLSA and RCLSB resistor values needed to set for PD class and the PD power consumption defined by standards. The PSE uses the number of class events and classification current information to classify the power requirement of the PD. The classification current includes the current drawn by RCLSA and RCLSB and the supply current of the devices so the total current drawn by the PD is within the IEEE 802.3bt standard. The classification current is turned off whenever the device is in power mode.
Table 1. PSE Type and PD Class with Classification Resistor RCLSA and RCLSB
PD CLASS
POWER REQUESTED BY PD
RCLSA
RCLSB
0
12.95W
619
OPEN
1
3.84W
118
OPEN
2
6.49W
66.5
OPEN
3
12.95W
43.2
OPEN
4
25.5W
30.9
30.9
5
38.25W
30.9
619
6
51W
30.9
118
7
61W
30.9
66.5
8
71W
30.9
43.2
Multi-Event Classification and Detection
IEEE 802.3bt defines physical classification to allow a PD to communicate its power classification to the connected PSE and to allow the PSE to inform the PD of the PSE’s available power. The PD classes (0~8) and PD power requests during Multi-Event Classification is configured by setting the RCLSA and RCLSB resistor values in Table 1. This configuration is compatible with IEEE 802.3af/at standard.
In a 1-Event classification, the PD is a 3af/at Class 0~3 PD. In a 2-Event classification, the PD is 3at Class 4 PD. In a 3-Event classification, the PD can be a 3bt PD at Class 0 to Class 4 depending on the classification current levels, and in this case the PD can take as high as 30W power from a 3bt PSE. In a 4-Event classification, the PD can be 3bt Class 5 PD with 45W, or 3bt Class 6 PD with 60W input power from PSE. If the third and fourth event the classification current are 10mA/20mA, it means PD power requests gets demotion from PSE. In a 5-Event classification, the PD can be 3bt PD Class 7 with 75W, Or a 3bt PD Class 8 with 90W input power from PSE.
Figure 1. Multi-Event Classification
Power Mode
The MAX5995A/MAX5995B/MAX5995C enter power mode when VIN rises above the undervoltage-lockout threshold (VON). When VIN rises above VON, the devices turn on the internal n-channel isolation MOSFET to connect VSS to RTN with inrush current limit internally set to 53mA (typ) when VRTN - VSS > 7V and 135mA (typ) when VRTN - VSS < 7V. The isolation MOSFET is fully turned on when the voltage at RTN is near VSS and the inrush current is reduced below the inrush limit. Once the isolation MOSFET is fully turned on, the devices change to the normal operation current limit. The open-drain power good output (PG) remains low for a tDELAY time (Electrical Characteristics) until the power MOSFET fully turns on to keep the downstream DC-DC converter disabled during inrush. Note that using larger output capacitors will result in longer start-up tDELAY time.
Power Demotion
The power demotion feature is provided for the situation where the power level PD requested is not available at the PSE. When power demotion occurs, the PD must operate in a reduced power mode while connected to lower power PSE. In Power Demotion mode, the PSE is going to provide the power that its classification indicates. For example, a 3af PSE only issue a single event even there is a Class 4 PD connected.
This feature is applicable in 4P PoE as well. For example, when a Class 5/6 PD connected to a PSE, the PSE only initiate 3-Event. It indicated the PSE supports 4P operation but can only deliver power up to 30W. Refer to Table 1 for more details.
Multi-Event Indication (MEC)
The device communicates its available power level to the system user through the MEC pin. The MEC pin state is a result of the number of classification/mark events, and whether the PD is in PoE or auxiliary power operation. The MEC pin can indicate power allocated from PSE to PD in 5 different cases.The devices uses a unique encoding method on the MEC pin to indicate the power levels that are higher than 12.95W. First pulse sent from MEC is START bit (256µs, 25% duty) for system to detect. Then the pattern of 2nd, 3rd, and 4th pulse width that is double or triple pulse width of the START bit (50% and 75% duty) is issued to indicate the type of PSE and power allocated from PSE. This pulse train is repeatable at certain frequency.
Number of event and the maximum power granted from the PSE at PD input are listed in Table 2. 1-Event and 2-Event are with IEEE802.3af/at standard. 3-Event, 4-Event, and 5-Event indicate PD Class (0~8) in IEEE802.3bt standard.
MEC is enabled after the isolation MOSFET is fully on until VIN drops below the UVLO threshold. The MEC is turned off when the device is in sleep mode and Ultra-Low-Power mode.
Table 2. MEC Pattern with Number of Events and PD Class
NUMBER OF EVENTS
MAXIMUM POWER GRANTED AT PD INPUT
1
12.95W
2 or Adapter
25.5W
3
25.5W
4
38.25W, if RCLSB = 619Ω; otherwise 51W
5
61W, if RCLSB = 66.5Ω; otherwise 71W
Figure 2. MEC Waveforms in Different Scenarios
Undervoltage Lockout
The MAX5995A/MAX5995B/MAX5995C operate up to a 60V supply voltage with a turn-on UVLO threshold (VON) at 35.4V and a turn-off UVLO threshold (VOFF) at 30V. When the input voltage is above VON, the devices enter power mode and the internal MOSFET is turned on. When the input voltage goes below VOFF for longer than tOFF_DLY, the MOSFET turns off.
Intelligent MPS
The intelligent MPS feature is provided by MAX5995B/MAX5995C. It enables applications that require low power standby modes. The MPS current is generated to comply with the IEEE 802.3bt standard for PSE to maintain power on in standby modes. A minimum current (10mA) of the port is able to be maintained with MPS mode to avoid the power disconnection from the PSE. The devices automatically enter MPS mode when the port current is lower than 24mA (typ) and exit MPS mode when the port current is greater than 28.7mA (typ).
Below drawing shows intelligent MPS behavior. The MPS comparator is autozero comparator and it will sample the port current every 32µs. The MPS comparator is always switched on when the MOSFET is fully turned on. If MPS comparator falling threshold is triggered continuously within 320µs, the part enters MPS mode and MPS current is generated. Once the part enter MPS mode it waits for the TMPS timer to elapse before check the MPS comparator again.
In MPS mode, Intelligent MPS modulation scheme is shown in Figure 3 (MPS Duty Cycle is 25% or 84ms), and the LED driver output (LED) sources periodic current pulses at 250Hz with 25% duty cycle and current amplitude can be configured by an resistor (RSL) on SL pin. PG remains high to enable downstream dc-dc converter in MPS mode. Once MPS mode is entered, sleep mode or Ultra-Low-Power sleep mode will not take effect (MAX5995B).
Figure 3. Intelligent MPS Behavior
Sleep and Ultra-Low-Power Sleep Modes (MAX5995A/MAX5995B)
The MAX5995A/MAX5995B feature a sleep mode, which pulls PG low to disable downstream DC-DC converters to minimize the power consumption of the overall PD system, while at the same time still keeps the internal MOSFET turned on and generate a MPS current at VDD to remain the PSE connection. However, when MAX5995B Intelligent MPS is enabled, and once the device enters MPS mode, sleep mode or Ultra-Low-Power sleep mode will not take effect. In sleep mode, the LED driver output (LED) sources a pulsating current and current amplitude can be configured by an external resistor (RSL) on SL pin. To enable sleep mode, apply a falling edge to SL pin (MAX5995B) or hold SL pin low for a minimum of 6 seconds after a falling edge (MAX5995A).
An Ultra-Low-Power sleep mode allows the MAX5995A/MAX5995B to further reduce power consumption while still maintaining pulsed MPS current required by standard at VDD. In Ultra-Low-Power sleep mode, the LED driver output (LED) sources periodic current pulses at 250Hz with 25% duty cycle and current amplitude can be configured by an resistor (RSL) on SL pin; the Ultra-Low-Power sleep enable input ULP is internally held high with a 50kΩ pullup resistor to the internal 5V bias of the MAX5995A/MAX5995B. To enable Ultra-Low-Power sleep mode, set ULP pin to logic-low and apply a falling edge to SL (MAX5995B) or hold SL low for a minimum of 6s (MAX5995A).
Apply a falling edge on the wake-mode enable input (WK) to disable sleep or Ultra-Low-Power sleep mode and resume normal operation. The PG pin is pulled low when the devices are in sleep mode or Ultra-Low-Power sleep mode, and pulled high once enable WK to resume normal operation.
Figure 4. MAX5995A/MAX5995B Sleep Mode Behavior (Not in MPS Mode)
The MAX5995A/MAX5995B drive an LED connected from the LED pin to VSS. During sleep mode and Ultra-Low-Power sleep mode, the LED pin sources periodic current pulses at 250Hz with 25% duty cycle. The current amplitudes in both cases can be programmed from 10mA to 20mA by the resistor connected from SL to VSS according to the following formula.
Power-Good Output
An open-drain output (PG) is used to allow disabling downstream DC-DC converter until the n-channel isolation MOSFET is fully turned on. PG is pulled low to VSS for a period of tDELAY and until the internal isolation MOSFET is fully turned on. Using larger output capacitors will result in longer tDELAY time. The PG is pulled low during sleep mode and Ultra-Low-Power sleep mode (in MAX5995A and MAX5995B not in MPS mode). PG is also pulled low in an overtemperature event and pulled high once the device comes out of thermal shutdown and resumes normal operation.
AUTOCLASS (MAX5995C)
In AUTOCLASS mode, the PSE is allowed to determine the actual maximum power consumption from the connected PD. When AUTOCLASS mode is enabled, during the first class event, the PD drops its current to class signature ‘0’ no earlier than 76ms (min) and no later than 87ms (max). The AUTOCLASS feature is only enabled in MAX5995C.
In AUTOCLASS mode, connect a resistor (no worse than 1% accuracy) between AUC and VSS to program the duty cycle of MPS current to further reduce the power consumption in MPS mode. There are four settings: floating (> 25%), 332kΩ (15%), 121kΩ (10%), and short to VSS (5%)
Table 3. AUC Configuration for MPS Current
AUC Pin Configuration
MPS Duty Cycle
AUC floating
> 25%
Connect 332k between AUC and VSS
15%
Connect 121k between AUC and VSS
10%
Short AUC to VSS
5%
The device will start a 82ms Timer On the first Classification Event. If the PSE does not provide the Long First Event, then the PD will not be in AUTOCLASS mode and will not modulate IMPS duty-cycle current according the AUC status. In this case, IMPS duty-cycle is the default value (> 25% pulses, as shown in Figure 6). If the PSE provide the Long First Event, the PD will truncate the classification current after 82ms to signature AUTOCLASS mode to the PSE, and then the PD will modulate the IMPS duty-cycle current according to AUC status. IMPS modulation scheme is shown in Figure 6.
Figure 6. MPS Current with Different AUC Configuration
Thermal-Shutdown Protection
The MAX5995A/MAX5995B/MAX5995C include thermal protection from excessive heating. If the junction temperature exceeds the thermal-shutdown threshold of +150ºC, the devices turn off the internal power MOSFET, LED driver, and MEC current sink. When the junction temperature falls below +120ºC, the devices enter startup mode and then power mode. Startup mode ensures the downstream DC-DC converter is turned off by pulling PG low until the internal power MOSFET is fully turned on.
Wall Power Adapter Detection and Operation
The devices feature wall power adapter detection for applications where an auxiliary power source such as a wall power adapter is used to power the PD by connecting it to WAD pin to RTN. Once the input voltage (VDD - VSS) exceeds the mark event threshold, wall adapter detection is enabled.The devices give the priority to the WAD and smoothly switch the power supply to WAD when wall adapter is detected. The devices detect the wall power adapter when the voltage from WAD to RTN is greater than 9V. When a wall power adapter is detected, the internal isolation MOSFET turns off, MEC current sink turns on to indicate certain pattern (see Multi-Event Indication (MEC)), the classification current is disabled if VIN is in the classification range, and the Intelligent MPS comparator is turned off.