Detailed Description

Detailed Description

The MAX40025 and MAX40026 are single-supply, high-speed comparators with a typical propagation delay of 280ps. The overdrive dispersion is extremely low (25ps, typ.), making these comparators ideal for time-of-flight distance measurement applications.

The input common-mode range of 1.5V to VDD + 0.1V is compatible with the outputs of several widely used high-speed transimpedance amplifiers, such as the MAX40658. The output stage is LVDS (Low-Voltage Differential Signaling), which helps to minimize power dissipation and interfaces directly with many modern FPGAs and CPUs.

The MAX40025 and MAX40026 operate from a +2.7V to +3.6V power supply voltage while typically consuming only 17mA quiescent current at 3.3V. The MAX40025 and MAX40026 are available in space-saving 6-WLP and 8-TDFN packages, respectively.

LVDS Outputs

Each LVDS output has a switched 3.25 mA current source. The outputs are differentially terminated with an external 100Ω resistor, which produces a ±350 mV differential output. The power delivered to the 100Ω load resistor is only 1.1mW while enabling transmission data rates up to a few hundreds of Megabits per second. The output common-mode voltage is maintained at 1.23 V on both outputs, and is independent of power supply voltage. The fully differential LVDS outputs provide high-speed digital signalling with reduced EMI compared to single-ended outputs.

System Timing Definitions
Table 1. Timing Definitions
SYMBOL SPECIFICATION DESCRIPTION
VOD Overdrive Voltage Differential voltage applied across inputs during test
tPDH Propagation Delay High on OUT+ Propagation delay measured from the time the differential input signal changes polarity (± input VOS) to the 50% point in the output low-to-high transition on OUT+
tPDL Propagation Delay Low on OUT- Propagation delay measured from the time the differential input signal changes polarity (± input VOS) to the 50% point in the output high-to-low transition on OUT-
ΔtPDHO Propagation Delay Skew on High Difference in propagation delay on output transition from low to high on OUT+ to propagation delay from high to low on OUT-
ΔtPDLO Propagation Delay Skew on Low Difference in propagation delay on output transition from high to low on OUT+ to propagation delay from low to high on OUT-
tR Output Rise Time Time taken by either OUT+ or OUT- to rise from 25% of final output voltage to 75% of final output voltage
tF Output Fall Time Time taken by either OUT+ or OUT- to fall from 75% of final output voltage to 25% of final output voltage
tPDL Propagation Delay Low on OUT- Propagation delay measured from the time the differential input signal changes polarity (± input VOS) to the 50% point in the output high-to-low transition on OUT-
tPDH Propagation Delay High on OUT- Propagation delay measured from the time the differential input signal changes polarity (± input VOS) to the 50% point in the output low-to-high transition on OUT-
tPDHD Differential Propagation Delay High Propagation delay measured from the time the differential input signal changes polarity (± input VOS) to the 50% point in the output differential signal across OUT+ to OUT- while switching low to high
tPDLD Differential Propagation Delay Low Propagation delay measured from the time the differential input signal changes polarity (± input VOS) to the 50% point in the output differential signal across OUT+ to OUT- while switching high to low
VOH Output Voltage High Comparator output high state voltage level
VOL Output Voltage Low Comparator output low state voltage level
Figure 1. System Timing Diagram
Propagation Delay

The propagation delay is defined as the delay between the differential comparator input voltage changing polarity and the output(s) reaching the mid-point of the high-to-low or low-to-high transition. The low-to-high propagation delay is tPDH on OUT+ and tPDH on OUT-, whereas the high-to-low propagation delay is tPDL on OUT+ and  tPDL on OUT-. These high-to-low and low-to-high timing parameters will differ slightly due to mismatches between the two complementary outputs. As a result, this difference in propagation delay is considered to be a skew for a given combination of low-to-high transitions on OUT+ and high-to-low transitions on OUT-.

Figure 2. Propagation Delay
Propagation Delay Dispersion
Dispersion, or variation of the propagation delay under different conditions, is affected by the amount of overdrive voltage applied to the comparator inputs. As can be seen in the Typical Operating Characteristics, the dispersion is typically under 25ps for 10mV to 1V, a wide range of input overdrive values.
Figure 3. Amplitude Overdrive Dispersion

Dispersion is also affected by the input slew rate. As the slew rate of the input signal changes, the propagation delay also changes. The dispersion is typically under 15ps from 0.4V/μs to 1V/μs input slew rates.

Figure 4. Slew Rate Dispersion
Hysteresis
Adding a small amount hysteresis to a comparator in a noisy environment is useful when input signals are slow-moving and have small noise levels superimposed on them. However, hysteresis must be used carefully when signals are small because it can cause valid signals to be ignored. Figure 5 shows the input signal and output response for a comparator with hysteresis applied.
Figure 5. Hysteresis Transfer Function

The MAX40025C is optimized for detecting very small, fast-changing signals and therefore has no internal hysteresis. The MAX40025A has fixed internal 2.5mV hysteresis and the MAX40026 has fixed internal 1.5mV hysteresis, which improves their usefulness for detecting larger differential input signals in the presence of noise. This helps to avoid the external components and potential stability degradation associated with external positive feedback paths.

Input Stage Circuitry

The MAX40025/MAX40026 include internal protection circuitry that prevents damage to the precision input stage from large differential input voltages. This protection circuitry consists of two groups of two front-to-back diodes between IN+ and IN-, as well as two 50Ω resistors (Figure 6). The diodes limit the differential voltage applied to the comparator’s internal circuitry to no more than 2VF, where VF is the diode’s forward-voltage drop (about 0.7V at +25°C).

For a large differential input voltage (exceeding 2VF), this protection circuitry increases the input bias current at IN+ (source) and IN- (sink).

INPUTCURRENT = VIN+ - VIN--2×VF2×50

Input currents with large differential input voltages should not be confused with input bias currents (IB). As long as the differential input voltage is less than 2VF , this input current is less than 2IB.

The input circuitry allows the MAX40025/MAX40026’s input common-mode range to extend 100mV beyond the positive power-supply rail. The output remains in the correct logic state if one or both inputs are within the common-mode range. Taking either input outside the common-mode range causes the input to saturate and the propagation delay to increase.

Figure 6. Input Stage Circuitry