The MAX20343/MAX20344 is designed to be compatible with small case-size ceramic capacitors. As such, the device has low-input and low-output capacitance requirements to accommodate the steep voltage derating of 0603 and 0402 (imperial) capacitors. The sample derating curve for a 22µF nominal value capacitor in Figure 7 presents the minimum capacitance required at IN and OUT. To ensure stability and low noise, the capacitance value under bias on IN should be the minimum of 5µF and the value of Figure 7 at the lowest expected VIN. The minimum capacitance value under bias on OUT should be equal to the value of Figure 7 at the lowest expected VOUT for BBstFETScale = 1 and twice that value for BBstFETScale = 0. Note that the derating curve in Figure 7 is a sample only, refer to the manufacturer’s derating curve of the actual capacitor selected to ensure that the minimum capacitance values under bias are met.
Inductor selection for the MAX20343/MAX20344 should be optimized for the intended application. A 2.2µH inductor value is required when FET scaling is enabled (BBstFETScale = 1) while 1µH is required when FET scaling is disabled (BBstFETScale = 0). Aside from the inductor value physical size, DC resistance (DCR), maximum average current, and saturation current are the primary factors to consider. The maximum average inductor current is obtained using the following equation:
Where,
VOUT_MAX is the maximum expected operating voltage,
IOUT_MAX is the maximum expected output current,
VIN_MIN is the minimum expected operating input voltage,
η is the expected worst case efficiency in the minimum input voltage and maximum output power case (see the Typical Operating Characteristics for help in estimating efficiency).
The average inductor current calculated above dictates the required maximum average current for temperature rise on the inductor. In order to determine the required inductor saturation current, the peak current must be calculated. The peak current for this converter can be calculated as:
Where BBstIPSet1 is the peak current setting described in register 0x03. When selecting an inductor, one primary factor in achieving high efficiency is the DCR of the inductor. For maximum efficiency, select an inductor with the lowest DCR possible in the required package size. Another factor to consider is magnetic losses. Generally magnetic losses are lower in inductors with larger physical size and/or higher saturation current ratings. In most cases ferrite inductors should be avoided as they tend to exhibit poor AC characteristics especially in discontinuous conduction mode (DCM).
When writing to the MAX20343/MAX20344 using I2C, the master sends a START condition (S) followed by the MAX20343/MAX20344 I2C write address. After the address, the master sends the register address of the register that is to be programmed. The master then ends communication by issuing a STOP condition (P) to relinquish control of the bus, or a REPEATED START condition (Sr) to communicate to another I2C slave. See Figure 8.
In this operation, the master sends an address and two data bytes to the slave device (Figure 9). The following procedure describes the single byte write operation:
- The master sends a START condition.
- The master sends the 7-bit slave address plus a write bit (low).
- The addressed slave asserts an ACK on the data line.
- The master sends the 8-bit register address.
- The slave asserts an ACK on the data line only if the address is valid (NACK if not).
- The master sends 8 data bits.
- The slave asserts an ACK on the data line.
- The master generates a STOP condition.
In this operation, the master sends an address and multiple data bytes to the slave device (Figure 10). The slave device automatically increments the register address after each data byte is sent, unless the register being accessed is 0x00, in which case the register address remains the same. The following procedure describes the burst write operation:
- The master sends a START condition.
- The master sends the 7-bit slave address plus a write bit (low).
- The addressed slave asserts an ACK on the data line.
- The master sends the 8-bit register address.
- The slave asserts an ACK on the data line only if the address is valid (NACK if not).
- The master sends 8 data bits.
- The slave asserts an ACK on the data line.
- Repeat 6 and 7 N-1 times.
- The master generates a STOP condition.
In this operation, the master sends an address plus two data bytes and receives one data byte from the slave device (Figure 11). The following procedure describes the single byte read operation:
- The master sends a START condition.
- The master sends the 7-bit slave address plus a write bit (low).
- The addressed slave asserts an ACK on the data line.
- The master sends the 8-bit register address.
- The slave asserts an ACK on the data line only if the address is valid (NACK if not).
- The master sends a REPEATED START condition.
- The master sends the 7-bit slave address plus a read bit (high).
- The addressed slave asserts an ACK on the data line.
- The slave sends 8 data bits.
- The master asserts a NACK on the data line.
- The master generates a STOP condition.
In this operation, the master sends an address plus two data bytes and receives multiple data bytes from the slave device (Figure 12). The following procedure describes the burst byte read operation:
- The master sends a START condition.
- The master sends the 7-bit slave address plus a write bit (low).
- The addressed slave asserts an ACK on the data line.
- The master sends the 8-bit register address.
- The slave asserts an ACK on the data line only if the address is valid (NACK if not).
- The master sends a REPEATED START condition.
- The master sends the 7-bit slave address plus a read bit (high).
- The slave asserts an ACK on the data line.
- The slave sends 8 data bits.
- The master asserts an ACK on the data line.
- Repeat 9 and 10 N-2 times.
- The slave sends the last 8 data bits.
- The master asserts a NACK on the data line.
- The master generates a STOP condition.
Data transfers are acknowledged with an acknowledge bit (ACK) or a not-acknowledge bit (NACK). Both the master and the MAX20343/MAX20344 generate ACK bits. To generate an ACK, pull SDA low before the rising edge of the ninth clock pulse and hold it low during the high period of the ninth clock pulse (Figure 13). To generate a NACK, leave SDA high before the rising edge of the ninth clock pulse and leave it high for the duration of the ninth clock pulse. Monitoring for NACK bits allows for detection of unsuccessful data transfers.
The following tables provide the device and register bit default values for the various available parts.
REGI STER BITS |
DEVICE | |||||||||
MAX
20343B
|
MAX 20343C |
MAX203 43E/ MAX203 44E/ MAX203 43O |
MAX 20343F |
MAX203 43G/ MAX203 43K |
MAX 20343H |
MAX 20343I |
MAX 20343J |
MAX 20343M |
MAX 20343N |
|
BBstEn | Disabled | Disabled | Disabled | Enabled | Disabled | Disabled | Disabled | Disabled | Disabled | Enabled |
BBst RampEn |
Single Step | Dig Ramp | Single Step | Single Step | Single Step | Single Step | Single Step | Single Step | Single Step | Single Step |
BBstFast | Low IQ Mode | Low IQ Mode | Low IQ Mode | Low IQ Mode | Low IQ Mode | Low IQ Mode | Low IQ Mode | Low IQ Mode | Low IQ Mode | Low IQ Mode |
BBstZCC mpDis |
ZCC Disabled | ZCC Disabled | ZCC Disabled | ZCC Disabled | ZCC Disabled | ZCC Disabled | ZCC Disabled | ZCC Disabled | ZCC Disabled | ZCC Disabled |
BBst LowEMI |
High Efficiency | High Efficiency | High Efficiency | High Efficiency | High Efficiency | High Efficiency | High Efficiency | High Efficiency | High Efficiency | High Efficiency |
BBstMode | Buck-Boost | Buck-Boost | Buck-Boost | Buck-Boost | Buck-Boost | Buck-Boost | Buck-Boost | Buck-Boost | Buck-Boost | Buck-Boost |
BBstAct Dsc |
Active Discharge on Shutdown (50ms) | Active Discharge on Shutdown (50ms) | Active Discharge on Shutdown (50ms) | Active Discharge on Shutdown (50ms) | Active Discharge on Shutdown (50ms) | Active Discharge on Shutdown (50ms) | Active Discharge on Shutdown (50ms) | Active Discharge on Shutdown (50ms) | Active Discharge on Shutdown (50ms) | Active Discharge on Shutdown (50ms) |
BBst PsvDsc |
Passive Discharge in Shutdown | Passive Discharge in Shutdown | Passive Discharge in Shutdown | Passive Discharge in Shutdown | Passive Discharge in Shutdown | Passive Discharge in Shutdown | No Passive Discharge | Passive Discharge in Shutdown | Passive Discharge in Shutdown | Passive Discharge in Shutdown |
BBstF HighSh [1:0] |
100kHz/25kHz | 100kHz/25kHz | 100kHz/25kHz | 100kHz/25kHz | 100kHz/25kHz | 100kHz/25kHz | 100kHz/25kHz | 100kHz/25kHz | 100kHz/25kHz | 100kHz/25kHz |
SwoFrcIN | Switch-Over Forced to VOUT when OutGood = 1 | Switch-Over Forced to VIN | Switch-Over Forced to VIN | Switch-Over Forced to VOUT when OutGood = 1 | Switch-Over Forced to VOUT when OutGood = 1 | Switch-Over Forced to VOUT when OutGood = 1 | Switch-Over Forced to VOUT when OutGood = 1 | Switch-Over Forced to VIN | Switch-Over Forced to VOUT when OutGood = 1 | Switch-Over Forced to VIN |
BBst VSet[5:0] |
3.20V | 5.00V | 5.00V | 3.30V | 3.20V | 3.30V | 4V | 2.85V | 3.20V | 5.00V |
BBst IntegEn |
Disable Integrator | Disable Integrator | Disable Integrator | Enable Integrator | Disable Integrator | Enable Integrator | Enable Integrator | Disable Integrator | Disable Integrator | Disable Integrator |
BBstIP AdptDis |
Adaptive Peak Current Enabled | Adaptive Peak Current Enabled | Adaptive Peak Current Enabled | Adaptive Peak Current Enabled | Adaptive Peak Current Enabled | Adaptive Peak Current Enabled | Adaptive Peak Current Enabled | Adaptive Peak Current Enabled | Adaptive Peak Current Enabled | Adaptive Peak Current Enabled |
BBst FETScale |
FET Scaling Enabled | FET Scaling Enabled | FET Scaling Enabled | FET Scaling Disabled | FET Scaling Enabled | FET Scaling Disabled | FET Scaling Disabled | FET Scaling Enabled | FET Scaling Enabled | FET Scaling Disabled |
FastRSEL Mode |
FAST | FAST | FAST | FAST | FAST | RSEL | RSEL | RSEL | FAST | RSEL |
EnI2C Mode |
I2C Control | EN Mode | I2C Control | I2C Control | I2C Control | EN Mode | EN Mode | EN Mode | I2C Control | EN Mode |
BBstIP Set1[3:0] |
100mA | 225mA | 225mA | 400mA | 100mA | 400mA | 300mA | 100mA | 100mA | 450mA |
BBstIP Set2[3:0] |
BBstIP Set1 + 200mA |
BBstIP Set1 + 150mA |
BBstIP Set1 + 150mA |
BBstIP Set1 + 600mA |
BBstIP Set1 + 200mA |
BBstIP Set1 + 600mA |
BBstIP Set1 + 350mA |
BBstIP Set1 + 225mA |
BBstIP Set1 + 200mA |
BBstIP Set1 + 300mA |
BBstIP 1SS[3:0] |
375mA | 375mA | 375mA | 750mA | 375mA | 750mA | 350mA | 375mA | 375mA | 375mA |
BBstIP 2SS[3:0] |
BBstIP Set1 + 75mA |
BBstIP Set1 + 75mA |
BBstIP Set1 + 75mA |
BBstIP Set1 + 150mA |
BBstIP Set1 + 75mA |
BBstIP Set1 + 150mA |
BBstIP Set1 + 100mA |
BBstIP Set1 + 75mA |
BBstIP Set1 + 75mA |
BBstIP Set1 + 75mA |
Slave_ Addr |
0xD0/0xD1 | 0xD0/0xD1 | 0xD0/0xD1 | 0xD0/0xD1 | 0xD0/0xD1 | 0xD0/0xD1 | 0xD0/0xD1 | 0xD0/0xD1 | xD8/0xD9 | 0xD0/0xD1 |
REGIST
ER |
NAME |
DEVICE | ||||||||||
MAX 20343B |
MAX 20343C |
MAX203 MAX203 |
MAX 20343F |
MAX203 43G/ MAX203 43M |
MAX 20343H |
MAX 20343I |
MAX 20343J |
MAX 20343K |
MAX 20343N |
MAX 20343O |
||
0x00 | ChipID | 0x02 | 0x02 | 0x02 | 0x02 | 0x02 | 0x02 | 0x02 | 0x02 | 0x03 | 0x03 | 0x03 |
0x01 | BBstCf g0 |
0x13 | 0x53 | 0x13 | 0x93 | 0x13 | 0x13 | 0x12 | 0x13 | 0x13 | 0x93 | 0x13 |
0x02 | BBstVS et |
0xCE | 0xF2 | 0xF2 | 0xD0 | 0xCE | 0xD0 | 0xDE | 0xC7 | 0xCE | 0xF2 | 0xF2 |
0x03 | BBstIS et |
0x84 | 0x69 | 0x69 | 0xC8 | 0x84 | 0xC8 | 0x76 | 0x94 | 0x84 | 0x69 | 0x69 |
0x04 | BBstCf g1 |
0x81 | 0xA1 | 0xA1 | 0x84 | 0x81 | 0x84 | 0x84 | 0xA1 | 0x81 | 0xA0 | 0xA1 |
0x05 | Status | 0x00 | 0x00 | 0x00 | 0x02 | 0x00 | 0x00 | 0x00 | 0x00 | 0x00 | 0x00 | 0x00 |
0x06 | Int | 0x00 | 0x00 | 0x00 | 0x00 | 0x00 | 0x00 | 0x00 | 0x00 | 0x00 | 0x00 | 0x00 |
0x07 | Mask | 0x03 | 0x03 | 0x03 | 0x03 | 0x03 | 0x03 | 0x03 | 0x03 | 0x03 | 0x03 | 0x03 |
0x50 | LockMsk | 0x01 | 0x01 | 0x01 | 0x01 | 0x01 | 0x01 | 0x01 | 0x01 | 0x01 | 0x01 | 0x01 |
0x51 | LockUn lock |
0xFF | 0xFF | 0xFF | 0xFF | 0xFF | 0xFF | 0xFF | 0xFF | 0xFF | 0xFF | 0xFF |