| 1 |
VDD |
Supply Input. Bypass VDD to ground with a 0.1µF capacitor. |
| 2 |
IN |
Monitoring Input. IN monitors for undervoltage/overvoltage faults with respect to nominal input threshold. When VIN falls outside the the undervoltage/overvoltage thresholds window, RST asserts and stays asserted for reset timeout period after VIN falls within undervoltage/overvoltage thresholds window. |
| 3 |
WDI |
Watchdog Input. The internal watchdog timer clears to zero on the falling edge of WDI or when RST goes high. If WDI sees another falling edge within the factory-trimmed watchdog window, WDO will remain de-asserted. Transitions outside this window, either faster or slower, will cause WDO to pulse low. WDI must not be left floating. Connect to ground with 100kΩ resistor to ensure proper device operation. See Window Watchdog Operation for more detail. |
| 4 |
GND |
Ground
|
| 5 |
CLR |
Clear Input. Pull CLR low for a pulse duration of tCLR to clear the overvoltage fault output at (OV) after the overvoltage condition is removed. CLR has a 50kΩ internal pull up to VDD. |
| 6 |
WDO |
Open-Drain Watchdog Output. WDO asserts low for 50ms when two consecutive falling transitions on WDI are shorter than tWD_F. WDO asserts low for 100ms when two consecutive falling transitions on WDI is longer than tWD_S. See Window Watchdog Operation for more detail. |
| 7 |
RST |
Open-Drain Reset Output. RST asserts low when VIN falls outside of the undervoltage/overvoltage threshold's window. The reset output deasserts after the reset timeout period when VIN enters the undervoltage/overvoltage threshold's window. |
| 8 |
OV |
Overvoltage Fault Output. OV latches low when the voltage at IN exceeds the overvoltage threshold setting. To clear the latch, pull CLR low for tCLR pulse width duration. |
| - |
EP |
Exposed pad. Connect EP to GND to improve heat dissipation capability. Add thermal vias below the exposed pad. |